• humidity
  • Facebook
  • Twitter
  • XING
  • LinkedIn
  • Send Page URL

humidity

Case Study: Cold Storage Warehouse Moves to Integrated, Wireless Environmental Monitoring

Katja Hinz | Applications, Pressure, Temperature

One of the world’s largest big-box retailers has installed a network of WIKA IIoT Solutions Leap Sensors ® in its climate-controlled warehouse for the wireless monitoring of humidity, temperature, differential pressure, and other critical conditions. In …

Read more

GPU-2000: SF6 Tank for Handling, Replacement, and Cleaning

Josh Sizemore | SF6 Gas Solutions
Transformer substation

The level of humidity in SF 6 -insulated switchgear must be kept below its water saturation point. If the gas is too humid, it loses some of its insulating properties; corrosion and dangerous leaks can also occur. A complete SF 6  handling instrument monitors the …

Read more

How Humidity Affects a SF6 Gas-Insulated Switchgear

Josh Sizemore | SF6 Gas Solutions
Water droplets

Sulfur hexafluoride is the gas most commonly used as insulator in power transmission and distribution switchgear. Water, however, can negatively affect the dielectric capabilities of SF 6  gas. To prevent operational and safety issues, it is important to measure and …

Read more
Welcome to the WIKA blog

In our WIKA US blog you can expect many interesting articles on pressure, temperature, level and flow measurement, and also on the subject of calibration technology. Furthermore, there are various insights into the world of the WIKA group of companies – seen from different angles.

Most-read articles
  • The Main Fertilizer Types and an Overview of Their Chemical Processes
  • WIKA Introduces Revolutionary Liquid-Filled Gauge with Flexible Window
  • WIKA Customizes Direct Drive Pressure Gauges for Aerospace and Military Oxygen Systems

© 2026 WIKA Alexander Wiegand SE & Co. KG

  • Privacy policy
  • Legal notice