A pressure transmitter is essential for waterjet cutting, a highly effective and affordable method for slicing through a wide range of materials. WIKA’s HP-2 high pressure transducer enables high precision monitoring at pressures up to 15,000 bar (217,000 psi). A …
Pressure Transmitters
WIKA Partners with Phase IV Engineering to Offer Innovative IIoT Solutions
| Patrick McGrath | ApplicationsIn August 2020, WIKA made a majority investment in Phase IV Engineering. This latest partnership means the company is better poised than ever to offer customers the best in measurement technologies and Industrial Internet of Things (IIoT) solutions. Wireless …
Better Together: The Advantages of Using Two Interconnected Process Transmitters for Differential Pressure Measurement
| Robert Lukat | Know-how, LevelLiquid level monitoring reaches a new height with WIKA’s innovative solution: a system that uses two interconnected process transmitters for differential pressure measurement. This configuration is extremely precise, easy to install and use, and not susceptible to …
WIKA’s Industrial Pressure Sensors Offer Reliability, Adaptability, Long-Term Savings
| Robert Lukat | PressureMany industrial applications rely on electronic instruments to convert pressure measurement into standard signals. The A-10 and S-20 are robust industrial pressure sensors that minimize downtimes and creates less work for field technicians. Pressure …
Pressure Measurement and Diagnostics: WIKA’s Field-Proven Solution
| Jeff Placek | PressureWIKA was the first company to produce a true OEM pressure transmitter with self-diagnostics, designed specifically to meet the challenges of pressure measurement in mobile working machines. The MH-3 has been successfully tried in the field and is a proven solution …