Which ignition protection type is suitable for battery-operated pressure measuring instruments, which are increasingly being used in combination with a radio unit? WIKA has clearly answered this question for its portfolio: “Ex i”, i.e. intrinsic safety. This …
All posts by Jing Lyu
Advantages of in-situ calibration using the example of pressure switches
Jing Lyu | ApplicationsIn-situ calibration of measuring instruments is carried out in numerous industrial processes. The advantages are obvious: The instruments remain installed, so the process does not have to be opened. In this way, plant operators reduce the time and costs involved in …
Injectables: Pressure measurement without risk of contamination
Jing Lyu | ApplicationsInjectables are among the most sensitive products in the pharmaceutical industry. Sterility is essential during production. This is because the active ingredient enters the patient's body directly, bypassing the patient's natural defences. It is therefore important to …
Pressure monitoring for mobile tanks in pharmaceutical processes
Jing Lyu | ApplicationsPressure monitoring in mobile tanks is an important measuring task in the pharmaceutical industry. Among other things, it enables users to check whether the containers are leak-tight during transport. In the case of active ingredients, this is an absolute necessity. …
Safe pressure measurement in chlorine production
Jing Lyu | ApplicationsPressure measurement plays a central role in chlorine production, which is a safety-critical process. This is due to the fact that chlorine is highly reactive and can therefore easily trigger explosions in combination with organic substances. So it is important to …