Applications

Filter monitoring for seawater cooling in power plants

Jing Lyu | Applications
Power plants on the shore: Differential pressure transmitters monitor the filters for cooling water from the sea.

Power plants near the shore often use seawater for their cooling systems. Before entering the circuit, it undergoes a complex filtering process to prevent damage to the system caused by residues. Continuous filter monitoring of the seawater cooling system is essential …

Read more

Force transducers secure cable-stayed bridges

Natallia Lineva | Applications

Cable-stayed bridges span roads, valleys, rivers and straits all over the world. They carry countless vehicles around the clock, every day. Their stability depends, crucially, on the permanent load-bearing capacity of the stay cables. Their tension must therefore be …

Read more

Seawater desalination: WIKA as a solution partner

Jing Lyu | Applications
WIKA supports operators of seawater desalination plants as a solution partner.

In the global supply of drinking and industrial water, seawater desalination plays a crucial role. As a result, more and larger plants are being built – especially in arid regions. WIKA is available to the industry in this market segment as an experienced solution …

Read more

Sewage sludge: Using force measurement technology to monitor the thickening process

Jing Lyu | Applications

Sewage sludge is a product of wastewater treatment. The drier it is, the better it can be utilised downstream. The key basic treatment of the sludge takes place in the thickeners. Their operational safety, in turn, depends on reliable force measurement in the drive …

Read more

Level measurement for demanding biorefinery applications

Ansgar Baule | Applications

The production of biofuels is subject to demanding process conditions. These therefore also pose major challenges for level measurement in biorefineries. The instruments used in the core processes, depending on where they are used, must operate in hydrogen-containing …

Read more
Most-read articles
  • Certification for fire-protection applications
  • Pressure switches in booster pumps
  • Hydrogen and pressure sensors – What must be observed?
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
Accuracy Calibration Chemical Diaphragm seals Electrical connection Ex protection Filling height Force measurement Functional safety (SIL) Hydrogen Hydrostatic Hydrostatic level measurement IIoT International Measuring instruments Measuring point Measuring principles Measuring range Oil & Gas Operating conditions Pharmaceuticals & Biotechnology Pressure Pressure gauge Pressure measurement device Pressure sensor Pressure switch Process connection Process safety Processtransmitter Project Renewable energy Resistance thermometer Safety Social commitment Standards/approvals/directives Submersible pressure transmitter Subsidiary Sustainability Switching function Temperature Temperature effect Thermocouple Thermometer Type of pressure Valves & Controllers


© 2026 WIKA Alexander Wiegand SE & Co. KG

  • Privacy policy
  • Legal notice