Applications

Hydrogen refuelling: Temperature influences the filling process

Jing Lyu | Applications
When refueling with hydrogen, temperature is a critical parameter.

Hydrogen is playing an increasingly important role as an alternative energy source, including as a climate-friendly fuel for motor vehicles. Its physicochemical properties make the supply of H 2 to cars and commercial vehicles a challenge for measurement technology. …

Read more

Using a multipoint thermocouple to produce sustainable aviation fuel

Jing Lyu | Applications
Ein Rohrbündelreaktor ist eine entscheidende Station bei der Herstellung von nachhaltigem Flugkraftstoff. Die Temperaturüberwachung dort erfolgt per Stufen-Thermoelement.

Waste is valuable. Solid municipal waste, such as packaging, paper or food, can be used to produce fuel for aircraft, for example. During the production process, the control of exothermic reactions requires reliable and precise temperature monitoring. This requires a …

Read more

New Food: Biomass fermentation harbours complex measuring requirements

Jing Lyu | Applications
New food can be produced efficiently through biomass fermentation.

According to UN forecasts, ten billion people will be living on Earth by 2050. The food industry must find new ways to ensure that the growing world population can be fed sustainably. One of these is New Food. This involves biotechnological food ingredients produced …

Read more

Pressure monitoring at high temperature is a challenge

Jing Lyu | Applications
Drucküberwachung unter Hochdruck: Visbreaking-Anlagen sind Teil einer Erdölraffinerie.

Pressure monitoring at high temperature is a demanding measuring requirement. This requires a specially designed diaphragm seal. With model 990.45, WIKA offers such an instrument in its portfolio and was therefore awarded the contract by the operator of an oil …

Read more

Hydrostatic pressure test with a digital pressure gauge

Jing Lyu | Applications, Pressure
Hydrostatic pressure test with a digital pressure gauge

A hydrostatic pressure test is used as a proof of strength and leak tightness of containers and pipelines that hold liquids and gases. The procedure and documentation of such a test can be increased in efficiency by using digital pressure gauges. This is particularly …

Read more
Most-read articles
  • Certification for fire-protection applications
  • Pressure switches in booster pumps
  • Hydrogen and pressure sensors – What must be observed?
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
Accuracy Calibration Chemical Diaphragm seals Electrical connection Ex protection Filling height Force measurement Functional safety (SIL) Hydrogen Hydrostatic Hydrostatic level measurement IIoT International Measuring instruments Measuring point Measuring principles Measuring range Oil & Gas Operating conditions Pharmaceuticals & Biotechnology Pressure Pressure gauge Pressure measurement device Pressure sensor Pressure switch Process connection Process safety Processtransmitter Project Renewable energy Resistance thermometer Safety Social commitment Standards/approvals/directives Submersible pressure transmitter Subsidiary Sustainability Switching function Temperature Temperature effect Thermocouple Thermometer Type of pressure Valves & Controllers


© 2026 WIKA Alexander Wiegand SE & Co. KG

  • Privacy policy
  • Legal notice