Applications

Unique: Diaphragm pressure gauge for pharmaceutical industry

Jing Lyu | Applications
Diaphragm pressure gauges for the pharmaceutical industry

Requirement and solution − The following example from China shows WIKA's competence in the pharmaceutical sector: One of the biggest vaccine manufacturers in China urgently needed a safe and autoclavable pressure gauge in hygienic design for the production of an …

Read more

Diaphragm seals for stable flow measurement in deep seas

Jing Lyu | Applications
Diaphragm seals enable stable flow measurement in the deep sea

Diaphragm seals make it possible to adapt measuring instruments to even the most extreme conditions. One example is the deep-sea extraction of oil and natural gas. For offshore companies in this industry, a particular OEM company manufactures flow measuring systems …

Read more

Calibration of ultra-high pressures over the entire measuring range

Jing Lyu | Applications
Calibration of ultra-high pressure

The calibration of ultra-high pressures is a challenge. This is because conventional test instruments are only designed for pressures up to 1,000 bar. In many applications, however, sensors work with several times this value, for example in the automotive industry. If …

Read more

Pressure switches in booster pumps

Gaston Dorren | Applications
Pressure switches in booster pumps

The invention of the pump itself was a major breakthrough for mankind. It significantly simplified the supply of drinking water. With growing demands for a stable water supply, largely free from pressure fluctuations, and at the same time increasing demands on the …

Read more

SIL pressure switch: Safety in tyre manufacturing

Jing Lyu | Applications
SIL pressure switch: Safety in tyre manufacturing

Numerous industrial processes have an inherently high risk potential. Special pressure switches support the safety of people and the environment. Example: the vulcanisation of tyres for motor vehicles. To monitor this process, leading manufacturers use the model MW …

Read more
Most-read articles
  • Certification for fire-protection applications
  • Pressure switches in booster pumps
  • Hydrogen and pressure sensors – What must be observed?
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
Accuracy Calibration Chemical Diaphragm seals Electrical connection Ex protection Filling height Force measurement Functional safety (SIL) Hydrogen Hydrostatic Hydrostatic level measurement IIoT International Measuring instruments Measuring point Measuring principles Measuring range Oil & Gas Operating conditions Pharmaceuticals & Biotechnology Pressure Pressure gauge Pressure measurement device Pressure sensor Pressure switch Process connection Process safety Processtransmitter Project Renewable energy Resistance thermometer Safety Social commitment Standards/approvals/directives Submersible pressure transmitter Subsidiary Sustainability Switching function Temperature Temperature effect Thermocouple Thermometer Type of pressure Valves & Controllers


© 2026 WIKA Alexander Wiegand SE & Co. KG

  • Privacy policy
  • Legal notice