Diaphragm seals, also known as chemical seals or remote seals, are used for pressure measurements when the process medium should not come into contact with the pressurised parts of the measuring instrument. A diaphragm seal has two primary tasks: 1. Separation of …
Products
The design of a submersible pressure transmitter / level probe – Part 1
Enrico Bossart | LevelA submersible pressure transmitter or level probe is a hydrostatic pressure sensor, specifically developed for the purpose of level measurement. Submersible pressure transmitters are level sensors with special characteristics and specific technical features, which …
Hydrostatic level measurement in closed geometries – calculation of the filling height
Enrico Bossart | LevelIn a previous blog post, I explained the calculation of the filling height in open geometries and vessels . Unlike open vessels, the calculation of level in closed geometries, such as gas-tight tanks or pressurised vessels, requires a compensation of the pressure of …
Hydrostatic level measurement in open geometries and vessels – calculation of the filling height
Enrico Bossart | LevelIn my last blog post, I introduced the way in which hydrostatic level measurement works . The hydrostatic pressure is used to determine the level through the measurement of the liquid column and is directly proportional to the filling height, as well as to the density …
How does hydrostatic level measurement work?
Enrico Bossart | LevelWhen considering a new level sensor for level measurement applications, it is often hard to find information on how the different types of level sensors, like the hydrostatic level sensors respectively hydrostatic pressure sensors, are working. Recently, I explained …