Vent valve instead of vent hole: With this option, the model PG43SA-S hygienic diaphragm pressure gauge is even suitable for pharmaceutical cleaning from the outside with particularly aggressive agents. The closed valve seals the inside of the pressure gauge in …
Products
Turning hydrogen into kilometres
Christian Wirl | PressureFuel cell electric vehicles (FCEV) powered by hydrogen are climate-friendly as well as powerful. The growing demand for these zero-emission drives is currently focused first and foremost on commercial vehicles. In Switzerland for example, the “H2 Mobility …
China Compulsory Certification (CCC) for electrical thermometers
Joachim Brückner | TemperatureThe “China Compulsory Certification (CCC)” is a certification system of the People's Republic of China. Since 1 October 2020 it is, for example, no longer permissible to place explosion-protected electrical thermometers (resistance thermometers and thermocouples) …
Check friction clutches using the chain hoist test set
Markus Heidl | ForceChain hoists are used for lifting and lowering freely moving loads. As a lifting device, the chain hoist supports, for example, ergonomic lifting during assembly work or even makes this possible in the first place. Conveyor technology or crane systems are further …
Dual range pistons for pressure calibration
Abhishek Sengupta | Calibration, ProductsDual piston deadweight testers can greatly enhance a lab’s ability to calibrate wide pressure ranges with the highest accuracy. With transducers and devices under test (DUTs) that have a wide measuring range, calibration can be a lengthy process, as you must change …