Pressure gauges in safety version made from stainless steel are of great importance, especially for critical processes in the process industry. They are recommended, for example, for applications with aggressive media and/or pulsations, overpressures and pressure …
EN 837
Pressure gauges and hydrogen: Which instruments are suitable?
| Christopher Ott | Pressure, ProductsPressure gauges play an important role in the production, storage, transport and use of hydrogen. In almost all applications, they monitor the pressure at measuring locations that require on-site indications which require no external energy, or serve as a backup for …
Integration of a pressure sensor element – error compensation of signal for zero point and span
| Christian Wirl | Know-howThe installation of a sensor element or a corresponding assembly has the advantage that very compact dimensions are possible. However, some points need to be taken into account, which are an additional effort for the customer compared to using a fully adjusted sensor …
Overload safety of Bourdon tube pressure gauges
| Marc Syguda | Know-howThe question occasionally arises, in connection with Bourdon tube pressure gauges, about the overload safety of the instruments. This article deals with exceeding the measuring range by up to 30 %. What happens with the pressure gauge? Does it still indicate precisely …
Traceability
| Matthias Bundschuh | Know-howMeasuring instruments for pressure and temperature are used in almost all areas of industrial manufacturing. As a result of continuous mechanical, chemical and thermal loading, these instruments age and can therefore not guarantee the correctness of the measured values …