New look plus enhanced functionality: WIKA has given its stainless steel pressure gauges and mechanical thermometers a comprehensive facelift. Customers benefit from this in several ways and at no extra cost. For example, they can use a QR code on the dial to open a …
Pressure gauge
Pressure monitoring at high temperature is a challenge
Jing Lyu | ApplicationsPressure monitoring at high temperature is a demanding measuring requirement. This requires a specially designed diaphragm seal. With model 990.45, WIKA offers such an instrument in its portfolio and was therefore awarded the contract by the operator of an oil …
Coatings of measuring instruments: Use and advantages
Sina Odenwald | Know-howProcess applications are becoming increasingly complex. Measuring instruments must therefore meet the highest requirements and function reliably – even with harsh outdoor conditions or aggressive media. Coatings are usually indispensable for use, for example, in the …
Injectables: Pressure measurement without risk of contamination
Jing Lyu | ApplicationsInjectables are among the most sensitive products in the pharmaceutical industry. Sterility is essential during production. This is because the active ingredient enters the patient's body directly, bypassing the patient's natural defences. It is therefore important to …
Saving sea lions with the help of WIKA pressure gauges
Stefan Schneider | WIKA insightWIKA pressure gauges fulfil an important task in the rescue of sea lions in Mexico – just one example of how unusual the possible applications of WIKA products can be. Sea lions inhabit the Baja California peninsula. However, their population is endangered by …