Requirement and solution − The following example from China shows WIKA's competence in the pharmaceutical sector: One of the biggest vaccine manufacturers in China urgently needed a safe and autoclavable pressure gauge in hygienic design for the production of an …
Pressure measurement device
Safe pressure monitoring for vaccine production
Silvia Weber | PressureIt can take up to three years to turn bacteria, viruses or cell cultures into a vaccine. Since vaccines are injected directly into the body, safety and purity have the highest priority in production. The demands on the plant equipment are correspondingly high, for …
Safe filter monitoring with differential pressure gauges
Jing Lyu | ApplicationsFilter monitoring is a core task of differential pressure gauges - the differential pressure increases as soon as the filter becomes clogged. The measuring instruments thus signal when the filter needs to be cleaned or replaced. The efficiency of such a solution can be …
Hygienic pressure gauge: IP68 with cleaning from the outside
Silvia Weber | ProductsVent valve instead of vent hole: With this option, the model PG43SA-S hygienic diaphragm pressure gauge is even suitable for pharmaceutical cleaning from the outside with particularly aggressive agents. The closed valve seals the inside of the pressure gauge in …
Pressure and temperature measurement at extremely low ambient temperatures
Christopher Ott | Know-howStandard pressure gauges and thermometers generally cope with ambient temperatures down to -40 °C. But what must be the features of a mechanical measuring instrument that works perfectly well in polar climates with even lower temperatures? This can be explained using …