If the careful use of “energy” as a resource used to be for cost reasons, today there is also increased environmental awareness. All of this also becomes mandatory thanks to legal requirements and the state of the technology. In this article you can read about how …
Pressure measurement device
Combination of pressure measuring instrument with accessories – Hook-up instead of own assembly
July Yang | Know-howPressure transmitters and pressure gauges can be adapted to almost any process condition using valves, protective devices and/or fittings. WIKA offers such combinations in the form of a "hook-up", an application-specific and ready-to-install solution. It eliminates all …
Against overheating: Differential pressure gauges as flow monitors
Manuel Schwestka | Know-howDifferential pressure gauges are not only suitable for the typical applications such as monitoring and control of filters or pumps. They can take on the function of a flow monitor, for example, in heat transfer oil plants. They thus control the volume flow of the …
DirectDrive pressure gauges – features and application areas
Sandra Broßler | PressureDirectDrive pressure gauges differ in structure and function from standard pressure gauges. Thus they feature special characteristics that qualify them for specific application areas. In DirectDrive pressure gauges, special pressure elements are fitted, which …
Selection criteria for digital indicators
Anna Zeitler | Know-howIn many electronic pressure measurement applications there is a need to have the measured value displayed on site - either as an additional option alongside the processing of the signal within the control system or as a sole control instrument. If the transmitter …