The model DMSU22SA in-line process transmitter from WIKA marks a new chapter for pressure monitoring in sanitary applications. The robust instrument with EHEDG certification and 3-A marking increases process reliability and, at the same time, reduces the consumption of …
Process safety
Pressure monitoring for mobile tanks in pharmaceutical processes
Jing Lyu | ApplicationsPressure monitoring in mobile tanks is an important measuring task in the pharmaceutical industry. Among other things, it enables users to check whether the containers are leak-tight during transport. In the case of active ingredients, this is an absolute necessity. …
Safe pressure measurement in chlorine production
Jing Lyu | ApplicationsPressure measurement plays a central role in chlorine production, which is a safety-critical process. This is due to the fact that chlorine is highly reactive and can therefore easily trigger explosions in combination with organic substances. So it is important to …
Diaphragm seal system with IO-Link, for the food industry
Tobias Hench | Pressure, ProductsThe DSSA11SA diaphragm seal system with IO-Link enables companies in the food industry to carry out smart pressure measurement. The WIKA instrument meets the high requirements of hygienic standards. It also supports the pursuit of continual improvement and …
Pressure switch for safe operation of food silos
Jing Lyu | ApplicationsPressure switches in food silos make a significant contribution to detecting overpressure in good time and safely preventing it. A manufacturer of such elevated vessels uses the model MA mechanical pressure switch for this task. One special property tipped the scales …