Temperature

Biofuels and e-fuels as a boost for many engines

Ansgar Baule | Applications
Biofuels and e-fuels are renewable alternatives to fossil fuels. Their production requires sophisticated measuring systems.

Biofuels and e-fuels are important building blocks in the global quest for a sustainable energy future. They are renewable and also promising alternatives to fossil fuels, as they reduce CO 2 emissions by up to 95 percent in comparison. WIKA has been supporting …

Read more

“Green” ammonia drives decarbonisation forward

Lukas Rothermich | Applications
The production processes for “green” ammonia demand tailor-made measuring systems.

“Green” ammonia is an ideal energy carrier. Being free of carbon, it offers a highly interesting potential for the future. As a typical building block of the “power-to-X” principle, “green” ammonia contributes to driving decarbonisation – in particular as …

Read more

Biofuels: Precise temperature profile for production

Jing Lyu | Applications
Biokraftstoffe haben einen zunehmenden Anteil am Energiemix.

Renewable instead of fossil: biofuels contribute significantly to climate protection and, in addition, to a more sustainable economy. They are produced, for example from used cooking oil, in reactors at temperatures of up to 450 °C. Monitoring these reactors requires …

Read more

Using IIot in a vineyard optimises frost protection

Thomas Hasenöhrl | Applications
An IIot solution in the vineyard optimises frost protection for the vines.

Climate change gives winegrowers a very hard time. Unforeseen weather events such as late frost or heavy rain can cause massive crop losses. The same is true for prolonged drought and moisture. Monitoring environmental conditions is therefore playing an increasingly …

Read more

Hydrogen refuelling: Temperature influences the filling process

Jing Lyu | Applications
When refueling with hydrogen, temperature is a critical parameter.

Hydrogen is playing an increasingly important role as an alternative energy source, including as a climate-friendly fuel for motor vehicles. Its physicochemical properties make the supply of H 2 to cars and commercial vehicles a challenge for measurement technology. …

Read more
Most-read articles
  • Certification for fire-protection applications
  • Pressure switches in booster pumps
  • Hydrogen and pressure sensors – What must be observed?
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
Accuracy Calibration Chemical Diaphragm seals Electrical connection Ex protection Filling height Force measurement Functional safety (SIL) Hydrogen Hydrostatic Hydrostatic level measurement IIoT International Measuring instruments Measuring point Measuring principles Measuring range Oil & Gas Operating conditions Pharmaceuticals & Biotechnology Pressure Pressure gauge Pressure measurement device Pressure sensor Pressure switch Process connection Process safety Processtransmitter Project Renewable energy Resistance thermometer Safety Social commitment Standards/approvals/directives Submersible pressure transmitter Subsidiary Sustainability Switching function Temperature Temperature effect Thermocouple Thermometer Type of pressure Valves & Controllers


© 2026 WIKA Alexander Wiegand SE & Co. KG

  • Privacy policy
  • Legal notice