A quarter of a century after its foundation in July 1999, WIKA Singapore can look back on an exciting success story. The subsidiary has evolved from a trading office to a process instrumentation solution hub that is serving customers locally, within ASEAN and even …
Calibration laboratory
Investments in India strengthen market position
Stefan Schneider | WIKA insightWith investments in India, WIKA has strengthened its position on the subcontinent. However, their purpose is not solely linked to the regional market – the subsidiaries there are also increasingly supplying companies in the wider WIKA Group. In Ghaziabad near …
Calibration laboratory brings WIKA Mexico forward
Stefan Schneider | WIKA insightAfter moving into new business premises back in 2018 and launching Axapta in 2019, WIKA Mexico is taking a further step this year: The calibration laboratory for pressure is being commissioned in accordance with Mexican standard NMX-EC-17025-IMNC-2018/ ISO/IEC 17025 …
Calibration bath or dry-well calibrator – which is the right choice?
Danica Schwarzkopf | Know-howTemperature sensors – like all other sensors – must be calibrated at regular intervals. This ensures that they deliver accurate and consistent measured values. Temperature calibration (e.g. using a calibration bath or dry-well calibrator) is generally carried out …
Dual range pistons for pressure calibration
Abhishek Sengupta | Calibration, ProductsDual piston deadweight testers can greatly enhance a lab’s ability to calibrate wide pressure ranges with the highest accuracy. With transducers and devices under test (DUTs) that have a wide measuring range, calibration can be a lengthy process, as you must change …