A diaphragm seal system with diaphragm monitoring from WIKA meets the highest safety requirements in sanitary applications. The model DMSU21SA with process transmitter and HART ® protocol (cover picture) can also be integrated into digitalised environments. Why …
Diaphragm seals
International competition: Torpedo drilled its way into the final
Stefan Schneider | WIKA insightBeing faster than a snail is a tremendous challenge for a tunnel boring machine. Students at DHBW Mosbach have mastered this, and have made it through to the final of an international competition with the “Dirt Torpedo”. WIKA co-sponsored the project by providing …
Flame arrester protects sewage vacuum truck tanks
Jing Lyu | ApplicationsA pre-volume deflagration flame arrester or – simplified – a flame arrester prevents flame transmission, through a measuring instrument, into a zone 0 (gas) hazardous area. This protective function, therefore, plays an important role, especially in process …
Diaphragm seals for stable flow measurement in deep seas
Jing Lyu | ApplicationsDiaphragm seals make it possible to adapt measuring instruments to even the most extreme conditions. One example is the deep-sea extraction of oil and natural gas. For offshore companies in this industry, a particular OEM company manufactures flow measuring systems …
Natural gas: On-site calibration optimised at the metering skid
Jing Lyu | ApplicationsOn-site calibration of measuring instruments is often very time-consuming and expensive. This is especially true for applications with several measurands. One example of this is the metering skid, a system for the custody transfer measurement of the amount of natural …