The model DMSU22SA in-line process transmitter from WIKA marks a new chapter for pressure monitoring in sanitary applications. The robust instrument with EHEDG certification and 3-A marking increases process reliability and, at the same time, reduces the consumption of …
Food/Beverages
NAMUR working group for pressure and temperature at WIKA
Stefan Schneider | WIKA insightThe NAMUR working group 3.11 (pressure and temperature) was a guest at WIKA. NAMUR are an international user association of automation technology and digitalisation in the process industry. The NAMUR working group started its two-day visit in May with a highlight: …
Diaphragm seal system with IO-Link, for the food industry
Tobias Hench | Pressure, ProductsThe DSSA11SA diaphragm seal system with IO-Link enables companies in the food industry to carry out smart pressure measurement. The WIKA instrument meets the high requirements of hygienic standards. It also supports the pursuit of continual improvement and …
Pressure switch for safe operation of food silos
Jing Lyu | ApplicationsPressure switches in food silos make a significant contribution to detecting overpressure in good time and safely preventing it. A manufacturer of such elevated vessels uses the model MA mechanical pressure switch for this task. One special property tipped the scales …
Level monitoring in milk tanks using a process transmitter
Jing Lyu | ApplicationsLevel monitoring using a process transmitter with a flush diaphragm is an option for applications in the food industry. It is highly accurate and at the same time suitable for aseptic tanks. A manufacturer of dairy products (milk, cream and yoghurt), for example, uses …