A hydrostatic pressure test is used as a proof of strength and leak tightness of containers and pipelines that hold liquids and gases. The procedure and documentation of such a test can be increased in efficiency by using digital pressure gauges. This is particularly …
Pressure
Pressure transducer: Digitally connected with EtherCAT®
Fabian Mayer | Pressure, ProductsPressure transducers with EtherCAT ® as the communication protocol continue the digitalisation of the semiconductor industry at the transmitter level. In future, in every production plant, dozens of pressure measuring locations will be equipped with them. Their …
Advantages of in-situ calibration using the example of pressure switches
Jing Lyu | ApplicationsIn-situ calibration of measuring instruments is carried out in numerous industrial processes. The advantages are obvious: The instruments remain installed, so the process does not have to be opened. In this way, plant operators reduce the time and costs involved in …
Injectables: Pressure measurement without risk of contamination
Jing Lyu | ApplicationsInjectables are among the most sensitive products in the pharmaceutical industry. Sterility is essential during production. This is because the active ingredient enters the patient's body directly, bypassing the patient's natural defences. It is therefore important to …
In-line process transmitter for sustainable pressure monitoring
Tobias Hench | Pressure, ProductsThe model DMSU22SA in-line process transmitter from WIKA marks a new chapter for pressure monitoring in sanitary applications. The robust instrument with EHEDG certification and 3-A marking increases process reliability and, at the same time, reduces the consumption of …