A basic pressure measuring device needs to be in contact with the media in a pipe, tubing or tank to determine the pressure. This technology works great for many applications; however, direct contact with hot or corrosive media can lead to damage or even destruction …
Applications
Instrumentation Matters When Reopening a Mothballed Plant
Robert Torgerson | ApplicationsReopening a mothballed plant offers a cost-effective alternative to new construction, but only if the overall structure is in good condition and major equipment is in good working order. It makes economic sense particularly if the plant's original design was flexible …
Little Things Can Cause Big Problems
Chad Reinhard | ApplicationsAn old nursery rhyme begins with the verse, “for the want of a nail.” Hard as it might be to believe, this fable has a lesson to teach about plant downtime and production efficiency. The rhyme offers a sequence of events involving a nail, a horseshoe, a horse, a …
Best Pressure Sensors for Heavy Equipment
Jeff Placek | Applications, PressureThe adage that “a chain is only as strong as its weakest link” works in many situations. In industrial applications, improper maintenance of electronic pressure sensors can cause heavy equipment to fail. Because pressure sensors tend to be installed deep …
The Importance of Wellhead Monitoring
Robert Lukat | ApplicationsWhy Is Wellhead Monitoring Important? Modern oil and natural gas wells are typically designed to operate unattended for extended periods. Downtime means lost profits, so oil companies are willing to pay a premium for rugged, reliable equipment for their wellheads. …