Applications

WIKA Provides Custom-Made Thermocouple Array for Contactor Column in a Chevron Refinery

Robert Torgerson | Applications, Temperature

WIKA designed a multipoint thermocouple array specifically for easy retrofitting into an existing amine contactor column at a Gulf Coast refinery. We customized the length so that there was a measuring junction at specific tray heights, then we threaded the array …

Read more

A WIKA–Chevron Partnership: Maximizing Amine Contactor Efficiency with Multipoint Temperature Systems

Robert Torgerson | Applications, Temperature

WIKA USA recently had the privilege of partnering with Chevron to custom-build multipoint thermocouple arrays for their refineries’ contactor columns. A chemical specialist from WIKA and a process control engineers from Chevron jointly  presented the following …

Read more

WIKA Provides Customized Hydrogen Pressure Sensors for Makers of Fuel Cell Systems

Jeff Placek | Applications, Pressure

WIKA has agreements with three US-based leaders in hydrogen mobility to supply them with customer-specific versions of our high-quality hydrogen-compatible pressure sensors for their fuel cell systems. The market for electric industrial vehicles continues to grow, …

Read more

How Multipoint Thermocouple Arrays in Amine Units Increase Production and Prevent Failures

Robert Torgerson | Applications, Temperature

Amine units are critical to the operations of refineries and chemical plants. If a unit fails due to corrosion, condensation and foaming, or another issue, the entire productivity and safety of the facility is imperiled. Temperature measurement solutions allow …

Read more

The Vital Role of Temperature in Amine Columns for Treating Natural Gas

Robert Torgerson | Applications, Temperature

The function of an amine unit is to remove unwanted sulfur compounds and carbon dioxide from raw natural gas before it is sold and used. Proper temperature control plays a crucial role in how well the amine solution absorbs acid gases, as well as prevent issues that …

Read more
Welcome to the WIKA blog

In our WIKA US blog you can expect many interesting articles on pressure, temperature, level and flow measurement, and also on the subject of calibration technology. Furthermore, there are various insights into the world of the WIKA group of companies – seen from different angles.

Most-read articles
  • The Main Fertilizer Types and an Overview of Their Chemical Processes
  • WIKA Introduces Revolutionary Liquid-Filled Gauge with Flexible Window
  • WIKA Customizes Direct Drive Pressure Gauges for Aerospace and Military Oxygen Systems

© 2026 WIKA Alexander Wiegand SE & Co. KG

  • Privacy policy
  • Legal notice