Calibration

Force Measurement & Calibration Solutions for the Pulp and Paper Industry

Chaz Marsinick

WIKA offers a complete selection of load pins, load cells, tension links, and force transducers for paper facilities, as well as portable equipment for the onsite calibration of pressure and temperature instruments. This article is a continuation of “ Pressure …

Read more

What to Know about Pressure Gauge Calibration

Ron Alexander
Pressure Gauge Calibration

Today’s pressure gauges are remarkably robust and accurate, but they do lose accuracy over time. Regular calibration of pressure gauges is the best way to ensure that readings are reliable. Different applications call for different levels of pressure gauge …

Read more

Two More Things for a Hydropower Plant To-do List: Force Measurement and Instrument Calibration

Jonathan Bey
Anchor Load Cell Mounting

Of course, hydroelectric power plants need to keep an eye on flow, level, temperature, and pressure. But don't forget about force, a key measurement as reservoirs are surrounded by rock and earth. There's also the matter of instrument calibration, an essential aspect …

Read more

When to Recalibrate Measuring Instrumentation

Hardy Orzikowski
Instrument calibration by WIKA

All measuring devices lose accuracy over time. Therefore, reliable readings require a regular schedule of calibrations. The particular conditions and needs of each application will determine when it is time to recalibrate a measuring instrument.   Time isn’t …

Read more

WIKA’s Calibration Lab receives ISO 17025 accreditation

Ron Alexander

Nearly all major manufacturers today understand the importance of having their manufacturing processes and products conform to comprehensive national and international standards. Larger nations typically have their own standards agency, and there are several …

Read more
Welcome to the WIKA blog

In our WIKA US blog you can expect many interesting articles on pressure, temperature, level and flow measurement, and also on the subject of calibration technology. Furthermore, there are various insights into the world of the WIKA group of companies – seen from different angles.

Most-read articles
  • The Main Fertilizer Types and an Overview of Their Chemical Processes
  • WIKA Introduces Revolutionary Liquid-Filled Gauge with Flexible Window
  • WIKA Customizes Direct Drive Pressure Gauges for Aerospace and Military Oxygen Systems

© 2026 WIKA Alexander Wiegand SE & Co. KG

  • Privacy policy
  • Legal notice