WIKA Temperature Transmitter Assemblies Receive Full FM Approval

Gabriel Gonzales | Temperature
temperature transmitter assembly

A product with FM Approval means it has undergone very rigorous testing and met extremely high standards for safety and reliability. That’s why WIKA was thrilled when our T15 and T16 temperature transmitter assemblies – not just certain components – received FM …

Read more

The Value of Using Averaging Resistance Temperature Detectors in HVAC Applications

Patrick McGrath | Temperature
Ventilation ducts

When it comes to HVAC temperature measurements, a single point sometimes is not enough. An averaging RTD measures temperature along a duct or across a sectional area, resulting in more accurate information about the overall conditions inside HVAC units.  …

Read more

WIKA’s iSENS HES Limit Switch Offers Unsurpassed Anti-Two Blocking Technology

Jeff Placek | Force
Anti-two block switch

A must-have component in lifting machinery, the anti-two block limit switch helps the operator protect equipment, loads, and personnel by preventing the hook block from colliding with the boom. WIKA Mobile Control manufactures the iSENS HES limit switch that is ideal …

Read more

Case Study: Unique Diaphragm Seal Assembly Meets Customer’s Precise Requirements

Chi-Che Ma | Pressure
Two-sided diaphragm seal assembly

A company in the energy and water/wastewater sector contacted WIKA about installing a diaphragm seal on a pipeline with limited clearance, but with a specific stipulation: The process gauge had to be readable from both sides. WIKA’s Diaphragm Seal Division designed a …

Read more

The Value of Ambient Temperature Monitoring in Industrial Plants

Gabriel Gonzales | Temperature
industrial plant

People, machinery, and products are best if they’re kept within a certain temperature range. Too much heat is especially a concern for equipment and perishables. That's why ambient temperature monitoring should be high on an industrial plant's to-do list. When …

Read more
Welcome to the WIKA blog

In our WIKA US blog you can expect many interesting articles on pressure, temperature, level and flow measurement, and also on the subject of calibration technology. Furthermore, there are various insights into the world of the WIKA group of companies – seen from different angles.

Most-read articles
  • Six Common Causes for Thermocouple Temperature Measurement Errors

  • Pt100 and Pt1000 Sensors: Important Facts and Differences

  • Where should I install my thermowell? A guide for best practices


© 2026 WIKA Alexander Wiegand SE & Co. KG

  • Privacy policy
  • Legal notice