Temperature sensors

Neither sensor is universally better. Choose a Pt100 for broad instrument compatibility and conventional industrial process applications. Choose a Pt1000 for two-wire installations, longer lead lengths, battery-powered equipment, and applications where lower self-heating is important.

Resistance temperature detectors (RTDs), also called resistance thermometers, are popular temperature measurement devices due to their reliability, accuracy, versatility, repeatability, and ease of installation.

The basic principle of an RTD is that its wire sensor – made of a metal with a known electrical resistance – changes its resistance value as the temperature rises or falls. Although resistance thermometers have certain limitations, including a maximum measuring temperature of about 1,100°F (600°C), overall they are the ideal temperature measurement solution for a multitude of processes.

Why Use a Platinum Sensor

The sensing wires in an RTD can be made of nickel, copper, or tungsten, but platinum (Pt) is by far the most popular metal used today. It’s more expensive than other materials, but platinum has several characteristics that make it particularly well suited for temperature measurements, including:

  • Almost linear temperature–resistance relationship
  • High resistivity (59 Ω/cmf compared to 36 Ω/cmf for nickel)
  • Non-degradable electrical resistance over time
  • Excellent stability
  • Very good chemical passivity
  • High resistance to contamination

To learn more about the relation between temperature and resistance in platinum RTD sensors, download our temperature table.

The Difference Between Pt100 and Pt1000 Sensors

Among platinum RTD sensors, Pt100 and Pt1000 are the most common. Pt100 sensors have a nominal resistance of 100Ω at ice point (0°C). Pt1000 sensors’ nominal resistance at 0°C is 1,000Ω. Linearity of the characteristic curve, operating temperature range, and response time are the same for both. The temperature coefficient of resistance is also the same.

However, due to the different nominal resistance, readings for Pt1000 sensors are higher by a factor of 10 compared to Pt100 sensors. This difference becomes evident when comparing 2-wire configurations, where lead measurement error is applicable. For instance, the measurement error in a Pt100 could be +1.0°C, and in the same design a Pt1000 could be +0.1°C.

How to Choose the Right Platinum Sensor

Both types of sensors work well in 3- and 4-wire configurations, where the additional wires and connectors compensate for the effects of the resistance of the lead wires on the temperature measurement. The two types are also similarly priced. Pt100 sensors, however, are more popular than the Pt1000 for a couple of reasons:

  • A Pt100 sensor comes in both wire-wound and thin-film constructions, offering users choice and flexibility. Pt1000 RTDs are almost always only thin-film.

  • Because their use is so widespread across industries, Pt100 RTDs are compatible with a large range of instruments and processes.

So, why would someone opt for the Pt1000 sensor instead? Here are the situations where the greater nominal resistance has the clear advantage:

  • A Pt1000 sensor is better in 2-wire configurations and when used with longer lead wire lengths.The fewer the number of wires and the longer they are, the more resistance is added to the readings, thereby causing inaccuracies. The Pt1000 sensor’s greater nominal resistance compensates for these added errors.
  • A Pt1000 sensor is better for battery-operated applications. A sensor with a higher nominal resistance uses less electrical current and, therefore, requires less power to operate. Lower power consumption extends battery life and the interval between maintenance, reducing downtime and costs.
  • Since a Pt1000 sensor uses less power, there is less self-heating. This means fewer errors in the reading as a result of higher-than-ambient temperatures.

In general, Pt100 temperature sensors are more commonly found in process applications, while Pt1000 sensors are used in refrigeration, heating, ventilation, automotive, and machine building applications.

When to choose a Pt100 vs. Pt1000 resistance thermometer (RTD)

Application / requirementPt100Pt1000
When you have a two-wire configuration ✅
When you have a three- or four-wire configuration✅ 
When the application needs long lead wires (cable runs) ✅
For maximum compatibility with instruments and across applications✅ 
For greater precision in detecting small temperature changes ✅
When you want or prefer wire-wound construction✅ 
When there are self-heating limits ✅
When power consumption is not a consideration (process industries)✅ 
For wireless (battery-operated) and lower-power applications like IIoT ✅

Replacing RTDs: A Note About Industrial Standards

RTDs are easy to replace, but it’s not a matter of simply swapping out one for another. The issue that users must watch out for when replacing existing Pt100 and Pt1000 sensors is the regional or international standard.

The older U.S. standard states platinum’s temperature coefficient as 0.00392 Ω/Ω/°C (ohm per ohm per degree centigrade). In the newer European DIN/IEC 60751 standard, which is also used in North America, it’s 0.00385 Ω/Ω/°C. The difference is negligible at lower temperatures, but becomes noticeable at boiling point (100°C), when the older standard will read 139.2Ω while the newer standard will read 138.5Ω.

WIKA USA, Smart in Sensing

For help or advice when purchasing or replacing RTDs, contact the temperature measurement experts at WIKA USA.


9 Responses to
  1. Sally Giles

    Love this! Thank you for sharing!

  2. John Danahy

    Good article. Thank you for making it simple enough for me to understand.

  3. Jonathan Apperley

    Perfect article, you explain the facts and differences between pt100 and pt1000 perfectly

  4. John

    Many thanks for clearly explaining the differences

  5. Wilson

    What about the price difference between the two?
    is it significantly more expensive to get the pt1000 ?

    • Adam DeLancey

      Hey Wilson,
      There is generally not any difference in price between the two different elements.

  6. Dalene Sumner

    To the wika.us administrator, You always provide valuable feedback and suggestions.

  7. Finn Bain

    Dear wika.us owner, Thanks for the comprehensive post!


Leave a Reply

You must be logged in to post a comment.