Mechanical Pressure Switches: Options and Selection Criteria (Part 2)

Jeff Placek | Applications, Pressure

Mechanical pressure switches are reliable and low-cost. And with the variety of options available, they meet the requirements of many different applications. This blog summarizes common features and factors to consider when selecting a mechanical pressure switch.  …

Read more

Long-Term Planning with the Gayesco Flex-R® Multipoint System Enables Major Cost Savings

Robert Torgerson | Temperature

Temperature control is a critical factor for reactor vessels in the refining and chemicals industry. The catalysts that convert the process oil in these reactors work best in very specific temperature ranges, and too high or too low a temperature can have a noticeable …

Read more

Getting to the Bottom of a RTD Sensor Reading Delay

Gabriel Gonzales | Temperature
Resistance Thermometer

The process engineers at a major chemical manufacturer were stumped. They were regularly getting very poor response times from their process temperature sensors and simply could not figure out why. The response times to temperature changes were consistently close to 30 …

Read more

Magnetostrictive Float Technology is Superior to Guided-Wave Radar for Level Measurement of Foamy Liquids

Patrick McGrath | Level

Accurate level measurement is critical in industries ranging from pharmaceutical, food, and beverage to petrochemical manufacturing. Continuous manufacturing (24/7) depends on careful monitoring of the level of feed materials and process media in tanks, pipes, and …

Read more

WIKA Has a Solution for Tight Spaces When Replacing Glass Gauges

Patrick McGrath | Level

Consistent and reliable, magnetic level indicators are widely used in many sectors, including the petrochemical industry. The operation of these cost-effective instruments is simple and elegant: A float resides within a chamber that, most commonly, is attached to the …

Read more
Welcome to the WIKA blog

In our WIKA US blog you can expect many interesting articles on pressure, temperature, level and flow measurement, and also on the subject of calibration technology. Furthermore, there are various insights into the world of the WIKA group of companies – seen from different angles.

Most-read articles
  • The Main Fertilizer Types and an Overview of Their Chemical Processes

  • WIKA Introduces Revolutionary Liquid-Filled Gauge with Flexible Window

  • WIKA Customizes Direct Drive Pressure Gauges for Aerospace and Military Oxygen Systems


© 2026 WIKA Alexander Wiegand SE & Co. KG

  • Privacy policy
  • Legal notice