A butter-pad allows refineries to weld new thermocouples onto it rather than directly on the bare furnace tube, as repeated welding damages the tube’s integrity. However, using this weld overlay affects the accuracy of temperature readings. WIKA conducted a series of IR scans, CFD simulations, and tests to quantify the temperature deviations caused by using a butter-pad with tubeskin thermocouples.

Temperature monitoring is essential to the efficient operation of fired heaters. Accurate temperature readings allow refineries to operate with furnace tubes very close to the creep, and to minimize fouling and coking inside those tubes.

Tubeskin Thermocouples, Welding Issues, and Butter-Pads

Thermocouples are accurate, long-lasting temperature sensors. However, because tubeskin thermocouples (TSTCs) are subjected to extreme temperatures, their reliability is limited to a few turnaround cycles, after which they should be replaced. Herein lies the problem:

  1. TSTCs are typically welded onto the tube surface.
  2. Replacement TSTCs need to be installed near the failed TSTCs’ existing location.
  3. The metallurgy of certain tubes does not allow for welding after extended use.

Therefore, refineries are limited in their ability to weld new thermocouples directly onto bare tubes when old thermocouples fail.

One of the ways to overcome the furnace tube’s metallurgical limitations is with a butter-pad. This is a predefined thickness of weld material installed on the tube surface. The new TSTC is then mounted on this weld overlay rather than on the bare tube, thereby avoiding any issues with tube integrity or requiring extensive post-weld heat treatment (PWHT).

However, using a butter-pad has its own issues. We wanted to understand how much this extra layer of metal impacted temperature measurement accuracy.

Methodology: Testing the accuracy of TSTCs installed on a butter-pad

Radially (longitudinal) installed butter-pad

Circumferentially (transversal) installed butter-pad

The variables of this project:

  • Weld material of a fixed dimension and thickness, installed circumferentially (transversal) or radially (longitudinal)
  • Different emissivity values of the butter-pad
  • Thermocouples products installed on bare tube vs. butter-pad
  • Different operating conditions

Reference thermocouples

As a reference, we installed tested thermocouples with known accuracies. Peening is one of the most common ways to install reference TSTCs, as this gives the truest tube skin temperatures. However, the number of tests that we had planned would require many changeouts and drill holes, making this method infeasible.

One alternative to the peened-in method is the capacitance discharge method for attaching reference thermometers to the surface. We tested this alternative method by comparing its temperature readings to those of a peened-in thermocouple, and found that the average temperature deviation between the two to be ~1.1°F (0.5°C) under various firing and process conditions. As this deviation is small, we felt confident in using the capacitance discharge method to weld reference thermocouples to the butter-pad. Note: The fired heater at the WIKA R&D Center is repeatable within 1°F (0.5°C), based on the many benchmarking and profiling tests carried out on this unit.

Fig. 1: Transversal (left) and longitudinal butter-pad on furnace tubeskin, IR thermography (click to enlarge)

Test results: Butter-pad on bare tube

Before testing TSTCs installed on a butter-pad, we first needed to understand the temperature distribution of the butter-pads themselves. Using infrared (IR) scanning, we found that the temperature at the weld overlay surface is consistently about 4°F (2.2°C) higher than the bare tube (see Figure 1). Results from computational fluid dynamics (CFD) simulations matched closely with the test data (see Table 1).

 

Table 1: Temperature of bare tube vs. butter-pad, IR thermography and CFD simulation

No.

Firing
(MMBtu/hr)

Reference (bare tube)

Butter-pad (IR)

Butter-pad (CFD)

1

6.9

762°F

766°F

765°F

2

5.9

735°F

738°F

737°F

3

4.6

700°F

704°F

702°F

The butter-pad surface temperature was lower than expected for a metal with a 0.196″ (5mm) thickness. IR scanning revealed an emissivity value of 0.67 to match the temperature, and this was further validated with the CFD model of the setup. The CFD was run again, this time with an emissivity of 0.45 and 0.85, both at the maximum firing rate, to understand the impact of emissivity on the surface temperature.

As expected, when the butter-pad is more polished than the bare tube, its lower emissivity value resulted in a cooler surface temperature. The inverse is true: a less polished surface (higher emissivity value) resulted in a hotter surface temperature (see Table 2).

Table 2: Butter-pad temperature with varying emissivity values, CFD simulation

No.

Butter-pad
emissivity value

Butter-pad
temperature*

Butter-pad
temperature deviation

1

0.45

735°F

−27°F

2

0.67

764°F

+3°F

3

0.85

785°F

+23°F

* at the center

We found it interesting that the butter-pad’s temperature was not consistent across its surface. Rather, the temperature tended to be higher at the edges and cooler toward the center (see Figure 2).

Fig. 2: Butter-pad temperatures with varying orientations and emissivity values, CFD simulation

      Longitudinal variation with ε

    Transversal variation with ε

  • The variation from edges to center was more pronounced at ε = 0.45 than at ε = 0.85.
  • Maximum to minimum variations:
    15°F (between ε = 0.67 and ε = 0.45)
    4°F (between ε = 0.67 and ε = 0.85)
  • The center is cooler than the sides for all three emissivity values.
  • The variation from edges to center was less pronounced at ε = 0.45 than at ε = 0.85.
  • Maximum to minimum variations: 5°F (between ε = 0.67 and ε = 0.45) 9°F (between ε = 0.67 and ε = 0.85)
  • The center is hotter than the sides at ε = 0.85 and cooler than the sides at ε = 0.45.

The last CFD simulation we did was to understand the impact of hotter firing conditions on the butter-pad temperature as compared to the bare surface temperature (see Table 3).

Table 3: Bare tube vs. butter-pad temperatures at different firings, CFD simulation

No.

Firing (MMBtu/hr)

Bare tube

Butter-pad

1

6.9 [normal heat]

798°F

801°F

2

12.7 [high heat]

1,000°F

1,003°F

 The validated CFD model was used to simulate test-run conditions for which product test data are available for bare tube installation.

Test results: Thermocouple installed on butter-pad

After analyzing and validating the above data, we then ran simulations and actual tests on the performance of our thermocouple product welded on top of the butter-pad. Doing so helped us understand the butter-pad’s impact on sensor accuracy. The MMBtu/hour test points were kept the same to maintain a similar basis for comparison.

First, we tested the product, unshielded and shielded, on a bare tube (see Table 4).

Table 4: Temperature deviation of unshielded vs. unshielded TSTC on bare tube

No.

Firing
(MMBtu/hr)

Bare tube temperature

 

Temperature reading

Temperature deviation

1

6.9

797°F

unshielded TSTC

         800°F

+3°F

   shielded TSTC

         796°F

−1°F

2

12.7

1,001°F

unshielded TSTC

      1,004°F

+3°F

   shielded TSTC

         992°F

−9°F

The data show that both the unshielded and shielded sensors are accurate within the thermocouples’ standard limits of error (SLE) tolerance for both normal and high heat release.

Second, we tested the product, unshielded and shielded, installed on a butter-pad (see Table 5).

Table 5: Temperature deviation of unshielded vs. unshielded TSTC on butter-pad

No.

Firing
(MMBtu/hr)

Bare tube temperature

 

Temperature reading

Temperature deviation

1

6.9

797°F

unshielded TSTC

         817°F

+20°F

   shielded TSTC

         819°F

+22°F

2

12.7

1,001°F

unshielded TSTC

      1,027°F

+26°F

   shielded TSTC

      1,022°F

+21°F

Judging by the data, both the unshielded and shielded product read higher by ≥20°F when installed on a butter-pad vs. on a bare tube. It is worth mentioning that the particular products used in these tests are highly accurate when installed on bare tubes; thermocouples that are less accurate would see an even greater temperature deviation, depending on their design.

This is part one of “Tubeskin Temperature Measurement: How to Improve Tubeskin Thermocouple Accuracy on a Butter-Pad”

[contact-form-7 id=”14552″ title=”Blog Contact Form”]


Leave a Reply

You must be logged in to post a comment.