No other term is as misleading as "compensated temperature range". Let´s first begin with what is meant: The compensated temperature range is the temperature range in which the temperature error, and accordingly the temperature coefficients, are valid. Not, as one …
All posts by Michèle Beyer
What is volume weight?
Michèle BeyerOr why it is important to find the right packaging for each product. Next to the actual weight which can be determined by weighing, there is also a so-called "volume weight". This is used for calculating transport costs. In addition to the actual weight, the …
Terminal boxes and angular connectors with M12x1: scope of delivery or accessories?
Michèle BeyerWe are often asked whether for instruments with M12 x 1 connector the corresponding mating connector (also called cable socket or angular connector) is included in the scope of delivery of our pressure sensors. Our clear answer is: no. Unlike the DIN connectors forms A …
Angular connector form A leaking/ loss of IP ingress protection
Michèle BeyerWhat are the rules that must be observed when assembling the angular connector EN 175301-803 A, to ensure that the IP rating is maintained, that is, connector and device remain really leak-tight? Unfortunately, a lot of things can go wrong when using the angular …
Aim and purpose of a vent hole in pressure sensors
Michèle BeyerIn so-called “gauge sensors” pressure is always measured relative to the currently prevailing ambient pressure. However, the ambient pressure is by no means constant. It is location- and height-dependent and changes with the weather. This means that for a …