Determining the weight of a mass requires a so-called load cell. Load cells are a special form of force transducer used to determine the weight force. This means that load cells are typically calibrated in weight units such as grams, kilograms or tonnes instead of the …
Weigh
How to build scales
Markus Heidl | Know-howDuring weighing, the weight force is measured, typically using scales. The mass is determined in two ways: comparatively or directly. As the goddess of justice in Roman mythology, Lady Justice is closely associated with Aequitas, the Roman law. Everyone knows her …