thermometer in sunlight

Especially the machine-building industry often asks me which is the right measuring element for them. This is the reason why I want to explain in this article the differences between the most commonly used sensors Pt100, Pt1000 and NTC. I will go into more detail about the lesser-used measuring elements Ni1000 and KTY sensors in the comparison at the end of this article.

Application areas of Pt100, Pt1000 and NTC

Resistance thermometers on the basis of Pt100, Pt1000 (positive temperature coefficient PTC) and NTC (negative temperature coefficient) are used everywhere in the industrial temperature measurement where low to medium temperatures are measured. In the process industry, Pt100 and Pt1000 sensors are used almost exclusively. In machine building, however, often an NTC is used – not least for cost reasons. Since meanwhile the Pt100 and Pt1000 sensors are manufactured in thin-film technology, the platinum content could be reduced to a minimum. As a result, the price difference compared to the NTC could be reduced to such an extent that a changeover from NTC to Pt100 or Pt1000 becomes interesting for medium quantities. Particularly since platinum measuring resistors offer significant advantages over negative temperature coefficients.

Advantages and disadvantages of the different sensors

The platinum elements Pt100 and Pt1000 offer the advantage of meeting international standards (IEC 751 / DIN EN 60 751). Due to material- and production-specific criteria, a standardisation of semiconductor elements such as NTC is not possible. For this reason their interchange ability is limited. Further advantages of platinum elements are: better long-term stability and better behaviour over temperature cycles, a wider temperature range as well as a high measurement accuracy and linearity. High measurement accuracy and linearity are also possible with an NTC, but only in a very limited temperature range. While Pt100 and Pt1000 sensors in thin-film technology are suitable for temperatures up to 500°C, the standard NTC can be used for temperatures up to approx. 150°C.

Influence of the supply line on the measured value

The lead resistance affects the measurement value of 2-wire temperature sensors and must be taken into account. For copper cable with a cross-section of 0.22 mm2, the following guide value applies: 0.162 Ω/m → 0.42 °C/m for Pt100. Alternatively, a version with Pt1000 sensor can be chosen, with which the influence of the supply line (at 0.04 °C/m) is smaller by a factor of 10. The influence of the lead resistance compared to the base resistance R25 for an NTC measuring element is far less noticeable. Due to the sloping characteristic curve of the NTC, the influence at higher temperatures increases disproportionately in case of higher temperatures.

Conclusion

In case of high quantities, the use of NTC sensors is still justified due to cost reasons. For small to medim-sized lots, I recommend the use of a platinum measuring resistor. The use of a Pt1000 manufactured in thin-film technology is a perfect compromise between the costs on the one hand and the measurement accuracy on the other. In the following table, I have compiled the strengths and weaknesses of the different measuring elements in an overview for you:

 Strengths and weaknesses of different sensors NTC Pt100   PT1000  Ni1000 KTY 
 Temperature range  – ++ ++ +  –
 Accuracy  – ++ ++ + – 
 Linearity –  ++  ++  ++ 
 Long-term stability ++  ++  ++ 
 International standards –  ++  ++  – 
 Temperature sensitivity (dR/dT) ++  – 
 Influence of the supply line ++  – 

Characteristic curves of Pt100, Pt1000, NTC, KTY and Ni1000

The characteristic curves of the different measuring elements can be seen in the following overview:

Characteristic curves of Pt100, Pt1000, NTC, KTY and Ni1000

Characteristic curves of the different sensors

 

Note
Our temperature sensors for the machine-building industry are available with all common measuring elements. Further information can be found on the WIKA website. 

Find out more about the functionality of resistance thermometers with Pt100 and Pt1000 sensors in the following video:

 



Post a comment