Pressure measurement could be so simple: Installing a pressure gauge, pressure transmitter or IIoT measuring instrument with radio unit – done. But in many cases, a measuring location requires more components than just the measuring instrument, especially in the …
Products
Stainless steel pressure gauges: Facelift brings digital features
Christopher Ott | PressureNew look plus enhanced functionality: WIKA has given its stainless steel pressure gauges and mechanical thermometers a comprehensive facelift. Customers benefit from this in several ways and at no extra cost. For example, they can use a QR code on the dial to open a …
Hydrostatic pressure test with a digital pressure gauge
Jing Lyu | Applications, PressureA hydrostatic pressure test is used as a proof of strength and leak tightness of containers and pipelines that hold liquids and gases. The procedure and documentation of such a test can be increased in efficiency by using digital pressure gauges. This is particularly …
Ignition protection type Ex i for pressure measuring instruments with battery operation
Jing Lyu | Pressure, ProductsWhich ignition protection type is suitable for battery-operated pressure measuring instruments, which are increasingly being used in combination with a radio unit? WIKA has clearly answered this question for its portfolio: “Ex i”, i.e. intrinsic safety. This …
Pressure transducer: Digitally connected with EtherCAT®
Fabian Mayer | Pressure, ProductsPressure transducers with EtherCAT ® as the communication protocol continue the digitalisation of the semiconductor industry at the transmitter level. In future, in every production plant, dozens of pressure measuring locations will be equipped with them. Their …