Hydraulic valve actuators require pressure switches for safe operation. In control cabinets, usually two of these measuring instruments are installed. One switch is used to control the pump for the hydraulic pressure, while the second triggers an alarm if the pressure …
Oil & Gas
WIKA has inaugurated a new factory in Kazakhstan
Stefan Schneider | WIKA insightWIKA has put into operation a new factory in Kazakhstan. The factory is located in Atyrau at the Caspian Sea. It took the team responsible for the location only six months from the planning to the start of production – in other words: one of the shortest project …
NAMUR working group for pressure and temperature at WIKA
Stefan Schneider | WIKA insightThe NAMUR working group 3.11 (pressure and temperature) was a guest at WIKA. NAMUR are an international user association of automation technology and digitalisation in the process industry. The NAMUR working group started its two-day visit in May with a highlight: …
Stainless steel pressure gauge in safety version: Selection guide
Christopher Ott | Know-howPressure gauges in safety version made from stainless steel are of great importance, especially for critical processes in the process industry. They are recommended, for example, for applications with aggressive media and/or pulsations, overpressures and pressure …
TA Luft now follows ISO 15848-1 for fugitive emissions
Pratik R. Vishwakarma | Know-howTA Luft has been revised. For the prevention of fugitive emissions, the new version of the German directive now follows the international standard ISO 15848-1. Correspondingly, tests in accordance with TA Luft follow the same test parameters as those in the ISO …