A major U.S. refinery returns to the Gayesco brand for WIKA USA's quality products, accurate information, expert installation, and exceptional customer service, even though it had an existing Global Frame Agreement with the competing bidder. Back in 1989, Gayesco …
All posts by Robert Torgerson
The Importance of Dipleg Temperature Measurement in FCC Units
Robert Torgerson | Know-howFCC units are the “money makers” of gasoline refineries. The pressure is on for operators to avoid delays in startup and to keep the units up and running. Accurate dipleg temperature measurement and monitoring ensures appropriate conditions for startup and prevents …
Avoid Expensive False Trips with Reliable Thermocouple Assemblies
Robert Torgerson | TemperatureA false trip is when an instrument error, rather than an actual problem, sets off (“trips”) a safety alarm. All plant operators want to avoid false trips, especially the ones that lead to a full process shutdown – a very expensive scenario. WIKA’s SIL III …
Industrial Thermocouple Repair and Replacement
Robert Torgerson | TemperatureA thermocouple has no moving parts and is extremely robust. However, thermocouples do lose accuracy over time and can become damaged by overheating during use or by human error. With a TC96-R thermocouple assembly, you enjoy the flexibility of thermocouple replacement …
Long-Term Planning with the Gayesco Flex-R® Multipoint System Enables Major Cost Savings
Robert Torgerson | TemperatureTemperature control is a critical factor for reactor vessels in the refining and chemicals industry. The catalysts that convert the process oil in these reactors work best in very specific temperature ranges, and too high or too low a temperature can have a noticeable …