Temperature is the most measured and monitored parameter in residential, commercial, and industrial HVAC applications. As such, dependable instrumentation is a must. WIKA manufactures a comprehensive portfolio of high-quality dial thermometers for industrial HVAC …
HVAC
The Value of Using Averaging Resistance Temperature Detectors in HVAC Applications
| Patrick McGrath | TemperatureWhen it comes to HVAC temperature measurements, a single point sometimes is not enough. An averaging RTD measures temperature along a duct or across a sectional area, resulting in more accurate information about the overall conditions inside HVAC units. …
The Value of Ambient Temperature Monitoring in Industrial Plants
| Ravi Jethra | TemperaturePeople, machinery, and products are best if they’re kept within a certain temperature range. Too much heat is especially a concern for equipment and perishables. That's why ambient temperature monitoring should be high on an industrial plant's to-do list. When …
Measuring Instruments Are Key to Energy Efficiency in Air Handling Units
| Patrick McGrath | ApplicationsWhat consumes the most energy in homes, offices, and businesses? It’s not the lights, but ventilation and air conditioning systems. WIKA USA is the one-stop resource for measuring instruments that reliably monitor and regulate air handling units to reduce both …