Reforming reactions in syngas (synthesis gas) plants require high heat, which takes a toll on the lifespan of furnace tubes. The higher the temperature, the shorter the tube life. Using a simple formula based on temperature measurements over time, plant operators can …
thermocouple assembly
WIKA V-PAD® Tubeskin Thermocouples Provide Accurate, Reliable Temperature Measurement in Ethylene Steam Crackers
Gabriel Gonzales | TemperaturePetrochemical plants use steam crackers to convert ethane into more useful ethylene. This energy-intensive process calls for maintaining very high temperature measurement within a relatively narrow range. The conversion of ethylene is poor if the temperature is …
The Benefits of Sheathed Thermocouples
Gabriel Gonzales | TemperatureThermocouples are rugged and respond quickly to temperature changes. When sheathed, these temperature measurement instruments are extremely resistant to vibration, mechanical stresses, and aggressive/corrosive media. Because they’re small and highly bendable, …
FAQs About Thermocouple Selection: Grounded vs. Ungrounded
Gabriel Gonzales | TemperatureThermocouples come in either grounded or ungrounded variants, which refer to whether the measuring point is welded to the sheath (grounded) or not (ungrounded). There are benefits, but also some tradeoffs, of using grounded vs. ungrounded thermocouples. …
Industrial Thermocouple – How to Choose the Right One
Gabriel Gonzales | TemperatureIndustrial Thermocouple - choosing the right one. The answer to the question “what kind of thermocouple?” depends on several factors relating to the process to be monitored, such as its compatibility with the media/process environment, frequency and accuracy of …