A thermocouple has no moving parts and is extremely robust. However, thermocouples do lose accuracy over time and can become damaged by overheating during use or by human error. With a TC96-R thermocouple assembly, you enjoy the flexibility of thermocouple replacement …
Thermocouple
FAQs About Thermocouple Selection: Grounded vs. Ungrounded
Gabriel Gonzales | TemperatureThermocouples come in either grounded or ungrounded variants, which refer to whether the measuring point is welded to the sheath (grounded) or not (ungrounded). There are benefits, but also some tradeoffs, of using grounded vs. ungrounded thermocouples. …
Industrial Thermocouple – How to Choose the Right One
Gabriel Gonzales | TemperatureIndustrial Thermocouple - choosing the right one. The answer to the question “what kind of thermocouple?” depends on several factors relating to the process to be monitored, such as its compatibility with the media/process environment, frequency and accuracy of …
Long-Term Planning with the Gayesco Flex-R® Multipoint System Enables Major Cost Savings
Robert Torgerson | TemperatureTemperature control is a critical factor for reactor vessels in the refining and chemicals industry. The catalysts that convert the process oil in these reactors work best in very specific temperature ranges, and too high or too low a temperature can have a noticeable …
Managing Thermal Expansion in Liquid Level Measuring
Patrick McGrath | LevelManaging thermal expansion in liquid level measuring is a common issue in refinery and chemical applications that put level gauges outside the vessel or tank. In this configuration, the gauge is exposed to atmospheric conditions that may affect the temperature of the …